AXIS#.STOP
Description
This command stops drive motion. In torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.
If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.
The following table defines the behavior of AXIS#.STOP:
| Cmdsource | Opmode | Subopmode | Deceleration ramp defined by: |
|---|---|---|---|
| Service | Torque |
- | AXIS#.IL |
| Velocity | - | AXIS#.SM.DEC and AXIS#.SM.DEC | |
| Position | Service motion | AXIS#.SM.DEC and AXIS#.SM.DEC | |
| Motion tasking | AXIS#.MT.DEC | ||
| Homing |
AXIS#.HOME.DEC | ||
| Fieldbus |
Torque | - | Command has no effect. |
| Velocity | |||
| Position | |||
| Electronic Gearing | Position | - | AXIS#.GEAR.DECMAX |
| Analog | Torque | - | Command has no effect. |
| Velocity | |||
| Position |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.STOP | 0x5000 | 0xD | UDINT | - | - | wo | False |
| AXIS2.STOP | 0x5100 | 0xD | UDINT | - | - | wo | False |